Ethernet port configuration page

The
Ethernet
configuration page is available for
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers. Use the page to do the following actions:
  • View and configure the port and IP address settings for IPv4 or IPv6 (for
    Micro850
    L50E and
    Micro870
    L70E controllers only).
  • Obtain IP addresses automatically using Dynamic Host Configuration Protocol (DHCP) or manually configure IP settings, and then download it to the controller when in
    Program
    mode.
  • Open the communication diagnostics view.
  • Synchronize the settings in the controller with the
    Internet Protocol Settings
    in your project using the
    Download to controller
    or
    Upload from controller
    button.
  • Select and clear the
    Detect duplicate IPv4/IPv6 address
    checkbox to enable and disable duplicate IP address detection.
  • Turn on or turn off duplicate IP address detection for IPv4 or IPv6 (for
    Micro850
    L50E and
    Micro870
    L70E controllers only).
  • Configure port settings, such as mode and speed.
    If you change the
    Speed
    or
    Duplex Mode
    settings and then download changes to the controller,
    FactoryTalk Design Workbench
    disconnects the controller after the download. This only happens when using an Ethernet connection, not when using a USB connection.
  • Enable or disable the
    Modbus TCP
    server.
Ethernet configuration settings
Setting
Description
Diagnose
Opens the communication diagnostics view.
Diagnose
is available when the controller is online.
Port Settings
Port state
Enables or disables the Ethernet port. Disables the port prohibits both transmitting data and receiving data.
Options are:
  • Enabled
  • Disabled
The Ethernet port is disabled by default.
Auto-negotiate speed and duplex mode
Determines whether the controller will automatically negotiate the port's speed and duplex mode.
  • When selected, the controller automatically configures the port's speed and duplex mode.
  • When cleared, you must configure the port's speed and duplex mode.
The auto-negotiation function turned on by default with a default speed of 10 Mbps.
Internet Protocol (IP) Settings
Configure IPv4
Enables or disables IPv4.
FactoryTalk Design Workbench
supports using IPv4 to download or upload projects and controller configurations.
Options are:
  • Enabled
  • Disabled
IPv4 is enabled by default.
Obtain IP address automatically using DHCP
Enables or disables the DHCP server to obtain IP addresses automatically.
Options are:
  • Enabled
  • Disabled
It is enabled by default.
Configure IP address and settings
Enables the manual entry for the IPv4 address, Subnet mask, and Gateway address.
Options are:
  • Enabled
  • Disabled
It is disabled by default.
IP address
Identifies the IP address of the controller on an Ethernet/IP network. Incorrect ranges for Static IPv4 IP addresses are:
  • Broadcast or Zero IP, such as 255.255.255.255 or 0.0.0.0
  • IP addresses starting with 0 or 127, such as 0.
    xxx.xxx.xxx
    and 127.
    xxx.xxx.xxx
  • IP addresses ending with 0 or 255, such as
    xxx.xxx.xxx
    .0 and
    xxx.xxx.xxx
    .255
  • IP addresses in the range 169.254.
    xxx.xxx
    , such as IP addresses from 169.254.0.0 through 169.254.255.255
  • IP addresses from 224.0.0.0 through 255.255.255.255
When you configure the IP address manually, the box displays either of the following:
  • The IP address in the controller, when the controller is online and its settings align with the specified IP address parameter value
  • The entered IP address
Subnet mask
Separates the entered IP address into a network address and a host address.
  • When you use the DHCP server to obtain network addresses, the subnet mask is displayed when the controller is connected.
  • When configuring the network settings manually, you must enter the IP address, and then select the
    Subnet mask
    box to fill the value automatically.
If the subnet mask is not correct, you cannot build the program successfully.
Gateway address
Specifies the network address of the gateway that connects individual physical networks into a system of networks.
  • When you use the DHCP server to obtain network addresses, the gateway address is displayed when the controller is connected.
  • When configuring the network settings manually, you must enter the gateway address.
Detect duplicate IP address
Enables or disables duplicate IP address detection.
Options are:
  • Enabled
  • Disabled
It is enabled by default.
Configure IPv6 (for
Micro850
L50E and
Micro870
L70E controllers only)
Enables or disables IPv6. When selected, the IPv6 settings are available for configuration.
  • FactoryTalk Design Workbench
    supports downloading the configured IPv6 address to or uploading the configured IPv6 address from a supported
    Micro800
    controller.
  • Downloading or uploading projects to or from a supported
    Micro800
    controller using IPv6 is not supported.
Options are:
  • Enabled
  • Disabled
By default, IPv6 is disabled. Either IPv4 or IPv6 must be enabled.
Obtain IPv6 address automatically (for
Micro850
L50E and
Micro870
L70E controllers only)
Enables the automatic retrieving of IPv6 network addresses using DHCP.
Available when IPv6 is enabled.
Options are:
  • Enabled
  • Disabled
It is disabled by default.
Configure IPv6 address and settings (for
Micro850
L50E and
Micro870
L70E controllers only)
Enables the entries for
IPv6 address
, Subnet prefix length, and Gateway address.
Available when IPv6 is enabled.
Options are:
  • Enabled
  • Disabled
It is disabled by default.
IPv6 address (for
Micro850
L50E and
Micro870
L70E controllers only)
Identifies the IPv6 address for the controller on an EtherNet network.
IPv6 address is 128 bits long, represented as eight groups of four hexadecimal digits, separated by colons. For example, 2001:0db8:0000:0000:0000:0000:0000:0001.
The following IPv6 addresses are likely to be set to the
Micro800
controller:
  • The IP address you entered, which is one of the IPv6 addresses set for the controller.
  • The read-only IPv6 address set by the router. It shows the last known value. The address is always available, and it appears dimmed when the controller is offline.
  • The read-only IPv6 address set by the static or DHCP server. It shows the last known value. The address is always available, and it appears dimmed when the controller is offline.
  • The read-only Linked Local Address set by the firmware using the SLAAC (Stateless Address Autoconfiguration) method. It shows the last known value and is always available.
Subnet prefix length (for
Micro850
L50E and
Micro870
L70E controllers only)
Specifies the size of the network portion of the IPv6 address.
The valid subnet prefix length range is from 0 through 128.
For example, an IPv6 address 2001:0db8:85a3:0000:0000:8a2e:0370:7334 with a subnet prefix length of 64 means that the first 64 bits (2001:0db8:85a3:0000) identify the network portion, and the remaining 64 bits identify the host portion.
When configuring the network settings manually, enter the
IPv6 address
, and then click the
Subnet prefix length
box to auto fill the value. Otherwise,
Subnet prefix length
remains empty.
Gateway address (for
Micro850
L50E and
Micro870
L70E controllers only)
A gateway connects individual physical networks into a system of networks.
When configuring the network settings manually, enter the
IPv6 gateway address.
Detect duplicate IPv6 addresses (for
Micro850
L50E and
Micro870
L70E controllers only)
Enables and disables duplicate IPv6 address detection.
  • Enabled
  • Disabled
It is enabled by default.
Ethernet/IP
Inactivity timeout
Specifies the inactivity time period in seconds.
The value is from 60 through 3600. The default value is 120.
Modbus TCP
Server state
Turns on or turns off the Modbus TCP server.
The Modbus TCP server is turned off by default.
Ethernet - DNP3 Over IP
(available for 2080-L70E-24QBBN and 2080-L70E-24QWBN controllers)
DNP3 over IP
Turns on or turns off DNP3 over the Ethernet and configures the Ethernet-specific parameters for DNP3 when turned on.
The DNP3 service over Ethernet will be turned on after a restart.
Slave node address
Specifies the address of the controller on the DNP3 network. Each device on the network must have a unique address.
The node address ranges from 0 through 65519.
Enable master address validation
Determines from which node address the controller accepts client requests.
  • When turned on, the controller accepts commands from the DNP3 clients that are configured for client nodes from node 0 through node 4.
  • When turned off, the controller accepts client requests from any node addresses.
The node address ranges from 0 through 65519.
Enable self-address
Allows or prohibits any packets that contain the destination address 65532 (FFFCh) to be accepted and processed.
This provides a mechanism for a client to discover the configured address of the controller when connected point-to-point. In a networked environment, this checkbox must be left clear.
Master node address
Specifies the node address from which the controller accepts the requests when
Enable master address validation
is selected.
The node address ranges from 0 through 65519.
Master node 0
is available by default.
Enable access control for master IP address
Determines from which IP addresses the controller accepts DNP3 client requests.
  • When enabled, the controller accepts DNP3 client requests from the IP addresses that are configured for client IP addresses from
    Master IP address 0
    through
    Master IP address 4
    .
    • Master IP address 0
      is available whether
      Enable access control for master IP address
      is selected or not. Enter the IP address of the DNP3 client to which unsolicited responses are sent.
    • Master IP address 1
      through
      Master IP address 4
      are available when
      Enable access control for master IP address
      is selected. Enter the IP address from which the controller accepts DNP3 client requests. Configuring all 4 of them is not necessary.
  • When disabled, the controller accepts DNP3 client requests from any IP addresses.
The maximum number of client IP addresses for access control is 5.
End point type
Selects the endpoint type from one of the following:
  • Listening
    : Supports using a single TCP connection as a server, through which unsolicited responses can exclusively be transmitted. The connection is established by the DNP3 client. User Datagram Protocol (UDP) broadcasts are accepted.
    Listening
    is the default value.
  • Dual
    : Supports using single TCP connections as a server and a client. When a TCP server connection is not present, unsolicited responses are sent to the DNP3 client via the TCP client connection. UDP broadcasts are accepted.
  • Datagram only
    : DNP3 over Ethernet communication is exclusively accomplished via UDP. TCP connections are not supported.
Local port number (UDP)
Specifies the UDP port number on the controller that the DNP3 client uses for UDP broadcasts. This is used with any endpoint type.
The port number ranges from 0 through 65535. The default value is 20000.
Local port number (TCP)
Specifies the TCP port number on the controller that the DNP3 client connects to. This is used with a
Listening
or
Dual
endpoint.
The port number ranges from 0 through 65535. The default value is 20000.
Master UDP port number (Unsol)
Specifies the UDP port number on the DNP3 client to which the controller sends unsolicited responses. This is used with a
Datagram only
endpoint.
The port number ranges from 0 through 65535.
Master UDP port number (Init Unsol)
Specifies the UDP port number on the DNP3 client to which the controller sends its unsolicited null response with RESTART IIN bit set after a restart.
This is used with a
Datagram only
endpoint and
Send the initial unsolicited null response on restart
is selected on the
DNP3 Slave
tab.
The port number ranges from 0 through 65535.
Master TCP port number (Unsol)
Specifies the TCP port number on the DNP3 client to which the controller connects for unsolicited response.
This is used with a
Dual
endpoint and when the DNP3 client doesn't already have a TCP connection open with the controller.
The port number ranges from 0 through 65535. The default value is 20000.
Keep-alive interval
Specifies the time interval, in seconds, for the TCP keep-alive mechanism. If the DNP3 client does not send any communication on an open TCP connection within this timeout period, the controller initiates a DNP3 Data Link Layer status request. If no response is received within the confirmation time period, 10 seconds by default, the controller will end the TCP connection.
This is used with a
Listening
or
Dual
endpoint.
The value is from 1 through 65535. The default value is 10.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal