Synchronize Internet Protocol settings
Use the
Ethernet
configuration page to synchronize the settings in the
controller with the Internet Protocol (IP) settings in the FactoryTalk Design Workbench
project.The IP settings in
FactoryTalk Design Workbench
are compared to the settings in the controller
when the controller is connected and in Program
mode. If the settings
do not match, a message will show, telling that the settings are different.Two options are provided to synchronize the IP settings:
- Download the settings fromFactoryTalk Design Workbenchto the controller.
- Upload the settings from the controller toFactoryTalk Design Workbench.
The two options are not available when:
- The controller is offline.
- The controller is inRunmode.
- The IP settings in the controller andFactoryTalk Design Workbenchare the same.
- The controller is in run mode change mode.
Prerequisites
- The controller is inRemote programmode.
- The IP settings in the controller andFactoryTalk Design Workbenchare different.
To synchronize Internet Protocol settings
- InProject Organizer, double-click the controller to open the controller application workspace.
- In theControllertree, selectEthernet.
- On theEthernetconfiguration page, select one of the following:
- Download to controller
- Upload from controller
Provide Feedback