Communication diagnostics for system

When diagnosing system communications, the following table lists the statistics monitored and displayed in real time.
Communication diagnostics for system
Filed
Description
CIP connection Statistics
Active total
Displays the number of CIP Explicit messaging and I/O connections in use.
Active messaging
Displays the total number of CIP Explicit (Class 3 to Message Router) messaging connections in use.
Active I/O
Displays the total number of CIP I/O (Implicit - Class1) connections in use.
Maximum CIP connections
Displays the maximum number of CIP connections supported by the system.
Connections timeout
Displays the number of connections which become non-existed because of a timeout.
I/O Resource Utilization
I/O communications utilization (actual)
Displays the communication utilization bandwidth currently used by the I/O resource in the system.
I/O communications utilization (theoretical)
Displays the communication utilization bandwidth supposed to be used by the I/O resource theoretically.
I/O rate (actual)
Displays the actual PPS (Packets Per Second) at which I/O communication is happening.
I/O rate (theoretical)
Displays the theoretical PPS (Packets Per Second) at which I/O communication is supposed to happen.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal