Serial port configuration page

Configure the serial port settings to establish communication between a
Micro800
controller and a serial device.
Use the
Serial Port
configuration page to do the following actions:
  • Configure communication protocols for
    Micro820
    L20E,
    Micro850
    L50E, and
    Micro870
    L70E controllers.
  • Select the communication protocol for the serial port.
  • Configure the communication settings for the selected communication protocol.
Serial port configuration settings vary with the driver that you selected. Available drivers are as follows:
By default, these serial port settings are not available for a
Micro820
L20E controller that supports remote LCD. To make the settings available, remove the LCD overwrite for serial settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal