Remove remote LCD overwrite for serial port settings

By default, remote LCD settings overwrite the Common Industrial Protocol settings configured on the
Serial Port
configuration page for
Micro820
L20E controllers that support remote LCD.
Clear the
Configure the serial port for remote LCD
checkbox to remove the remote LCD overwrite for serial port settings.
To remove remote LCD overwrite for serial port settings
  1. In
    Project Organizer
    , double-click the controller to open the controller application workspace.
  2. In the
    Controller
    tree, select
    Remote LCD
    .
  3. On the
    Remote LCD
    configuration page, clear the
    Configure the serial port for remote LCD
    checkbox.
  4. Select the
    serial port
    link to open the
    Serial Port
    configuration page, and then configure the serial port settings as needed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal