Serial Port - Modbus RTU configuration page

Use the Modbus RTU configuration page to do the following actions:
The displayed configuration settings vary with the
Micro800
controller selection.
Modbus RTU configuration settings
Setting
Description
Common Settings
Diagnose
Opens the communication diagnostics view.
Diagnose
is available when the controller is online and
CIP Serial
or
Modbus RTU
is selected as the driver.
Baud rate
Lists the baud rate in bits per second. Options are:
  • 1200
  • 2400
  • 4800
  • 9600
  • 19200
  • 38400
The default baud rate is 19200.
Parity
Lists the parity bit usage in the communication packets. Options are:
  • None
  • Odd
  • Even
The default value is None.
Modbus role
Specifies the role of the Modbus port. Options are as follows:
  • Master
  • Slave
  • Auto
The default option is
Master
.
Unit address
Specifies the Unit ID if configured as a Modbus server (slave).
The option is not available when
Modbus role
is set as
Master
.
When you select
Slave
or
Auto
for
Modbus role
, the unit address is from 1 through 247. The default value is
1
.
For instance, in a scenario where the controller is set up as a Modbus RTU slave that is connected to a
PanelView™
Component (PVC), the PVC is the Modbus master and uses the address of 0.
Protocol Control
Media
Specifies the supported media types. Available options for
Micro850
L50E and
Micro870
L70E controllers are:
  • RS232
  • RS485
Control line
Specifies the type of handshake that is used for communication.
  • Select
    RTS/CTS
    if both the master and slave are using half-duplex modems.
  • Select
    No Handshake
    for direct point-to-point communication without a modem.
Data bits
Specifies the number of data bits per character. The value is 8 and is read-only.
Stop bits
Specifies the number of stop bits per character. Options include
1
and
2
. 1 is the default option.
Response timer
Specifies a Modbus master's minimum waiting time for a response from the Modbus slave before a new transmission can begin.
The value is from 0 through 4,294,967,295. The default value is 200.
In a scenario where the
Micro800
controller serves as a master of the Modbus RTU slave, to send a complete response, the value must be restricted within the required time from the slave.
Broadcast pause
Specifies the amount of time to delay after the data broadcast. The value is from 0 through 4,294,967,295. The default value is 200.
Inter-frame (delay/timeout)
Specifies the amount of time to delay after a transmission request. The value is from 0 through 4,294,967,295. The default value is 0.
RTS pre-delay
Specifies the amount of time to delay before requesting a transmission. The option is available when
Media
is set to
RTS32
and
Control line
is set to
RTS/CTS
.
The value is from 0 through 4,294,967,295. The default value is 0.
The option is available when
Media
is set to
RS232
and
Control line
is set to
RTS/CTS
.
RTS post-delay
Specifies the amount of time to delay after requesting a transmission. The option is available when
Media
is set to
RTS32
and
Control line
is set to
RTS/CTS
.
The value is from 0 through 4,294,967,295. The default value is 0.
The option is available when
Media
is set to
RS232
and
Control line
is set to
RTS/CTS
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal