Can't connect to Allen-Bradley PanelView Plus devices
RSLinx Enterprise or
FactoryTalk Linx
must be installed on the client computer to communicate with PanelView Plus operator interfaces. RSLinx Enterprise must be version 5.00 or higher, and FactoryTalk Linx
must be version 6.00 or higher. See the FactoryTalk AssetCentre Installation Guide
for information on installing RSLinx Enterprise or FactoryTalk Linx
.FactoryTalk View Machine Edition must be installed on the agent computer to communicate with PanelView Plus operator interfaces. This is a separate installation that is not included as part of the FactoryTalk AssetCentre installation.
Provide Feedback