Create searches

Use FactoryTalk AssetCentre Searches to show specified records from the Event Log, Audit Log, Diagnostics and Health Log, Archive History Log, the Archive Check In and Check Out Status, or the Asset Extended Property. Search results can be based on any column of data in a record and are generated based on complex conditions that you set. To query logs without using complex conditions or to be able to open record attachments from within search results, use Quick Search.
Prerequisites
  • To create searches, you must have the
    View a Search
    and
    Create a Search
    permissions.
  • To create scheduled searches, you must also be granted the
    Create a new schedule
    ,
    Edit a schedule
    ,
    View a schedule
    , and
    Command a schedule
    permissions.
To create a search
  1. Select
    View > Searches
    , or click the
    Searches
    button.
  2. Select
    File > New
    , or click the
    New
    button.
    TIP:
    You can also right-click any search row on the
    Searches
    tab and select
    New
    .
  3. Complete the
    New Search Wizard: Search Properties
    dialog box.
  4. To create an unscheduled search for the selected data source, click
    Finished
    and go to Step 6.
  5. To create a scheduled search to run later, click
    Schedule
    , complete the
    New Search Wizard: Timing Properties
    dialog box, and then click
    Finished
    .
  6. To configure how the search results will appear, complete the
    Source and Display
    tab. If you do not complete this tab, the default format will be used for the search results.
  7. To set the criteria to be used to search the record, complete the
    Conditions
    tab. If you do not complete this tab, there will be no conditions placed on the records returned in the search results.
  8. To format and modify the recipient list for scheduled search results and set the time zone for the computer running the search, complete the
    Scheduled Search Operation
    tab.
    TIP:
    The
    Scheduled Search Operation
    tab only appears when you select a scheduled search definition on the
    Searches
    tab.
  9. Run the search.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal