Starting point of a schedule

The starting point of a schedule is the top-level asset in the schedule. It is a asset, if the schedule is only for one asset, or it is a container that holds all the other assets in the schedule.
starting_point_of_schedule
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal