Rename a schedule

You might want to rename a schedule if you modify its operation properties or change when the schedule runs. FactoryTalk AssetCentre shows all schedules created in your system. Naming schedules can make filtering them easy. Before you can rename a schedule, the schedule must be inactive.
Prerequisites
  • To rename schedules, you must have
    Edit a schedule
    permission.
To rename a schedule
  1. Select
    View > Schedules
    , or click the
    Schedules
    button.
  2. Next to the desired schedule, clear the
    Active
    check box.
  3. Click in the
    Name
    field of the schedule, and then type the new unique name of the schedule.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal