Allen-Bradley PowerFlex Drive operation properties for disaster recovery
Following are all possible settings for disaster recovery schedules for Allen-Bradley
PowerFlex Drive assets.
These settings are used for two purposes:
- Specify default disaster recovery schedule settings for Allen-Bradley PowerFlex Drive assets inTools > Options.
- Specify the settings of a particular Allen-Bradley PowerFlex Drive asset in an existing schedule on theSchedulestab. Changes to the settings within a schedule override the default settings for that instance.
Unless noted otherwise, each setting applies to backup schedules and backup and compare schedules.
(Backup and compare schedules only) Event Settings
- Backup Compare Partner(Only available when editing an existing schedule, not when setting defaults.) Specify the version of the backup data binder to compare to the controller files.TIP:The compare report is generated, no matter whether there are differences found or not.
- Configuration Data Compare Partner(Only available when editing an existing schedule, not when setting defaults.) Specify the version of the configuration data binder to compare to the device files. For Allen-Bradley PowerFlex Drive, the configuration data is not compared during a backup and compare operation unless specified.
- Create New Backup VersionSet toAlwaysto create a backup version even if it is exactly the same as the last compared backup version. This is the default setting.Set toOn Differences Foundto create a backup version only if differences are found. If the existing backup is the same as the information in the controller aside from excluded data blocks, then no backup is saved.
Email notification
You can type email recipients' addresses separated by semicolons (;) or select addresses from the FactoryTalk AssetCentre Address Book. To select addresses from the Address Book, click in the field, and then click
. Complete the
. Complete the Contacts and Groups
dialog box.An email message will be sent to only one of these lists. For example, if differences are found when a backup and compare schedule runs, an email is sent to those on the
Event Compare Differences Detected
list. No email is sent to those on the Event Completed
list.- (Backup and compare schedules only) Event Compare Differences DetectedThe email addresses, separated by semicolons (;), to which notification will be sent if the compare finds differences between the specified backup data or configuration data version and the data on the physical device.
- Event CompletedThe email addresses, separated by semicolons (;), to which notification will be sent when the operation completes for the asset. If a backup and compare schedule completes without differences, an email is sent to this list. If it completes with differences, an email is sent to theEvent Compare Differences Detectedlist, not this list.
- Event FailedThe email addresses, separated by semicolons (;), to which notification will be sent if the operation fails.
(Backup and compare schedules only) Attach report to email
- Event Compare Differences DetectedThis defaults toTrueto attach a report of differences to the email if the backup and compare schedule finds differences between the specified backup data or configuration data version and the data on the physical device. SelectFalseto send an email without an attached report.
Provide Feedback