FactoryTalk Optix Runtime (Software) operation properties for disaster recovery
Following are all possible settings for disaster recovery schedules for FactoryTalk Optix
Runtime (Software) assets.
These settings are used for two purposes:
- Specify default disaster recovery schedule settings for FactoryTalk Optix Runtime (Software) inTools > Options.
- Specify the settings of a particular FactoryTalk Optix Runtime (Software) asset in an existing schedule on theSchedulestab. Changes to the settings within a schedule override the default settings for that instance.
Unless noted otherwise, each setting applies to backup schedules and backup and compare
schedules.
(Backup and compare schedules only) Event Settings
- Backup Compare Partner(Only available when editing an existing schedule, not when setting defaults.) Specify the version of the backup data file to compare to the FactoryTalk Optix Runtime (Software) asset files.TIP:The compare report is generated, no matter whether there are differences found or not.
- Create New Backup VersionSet toAlwaysto create a backup version even if it is exactly the same as the last compared backup version. This is the default setting.Set toOn Differences Foundto create a backup version only if differences are found. If the existing backup is the same as the information in the FactoryTalk Optix Runtime (Software) asset, then no backup is saved.
Asset specific properties
- Only Report DifferencesSet toTrueto generate a report that only shows differences when differences are found and the task is completed successfully.
Email notification
You can type email recipients' addresses separated by semicolons (;) or select addresses from the FactoryTalk AssetCentre Address Book. To select addresses from the Address Book, click in the field, and then click
. Complete the
. Complete the Contacts and Groups
dialog box.An email message will be sent to only one of these lists. For example, if differences are
found when a backup and compare schedule runs, an email is sent to those on the
Event
Compare Differences Detected
list. No email is sent to those on the Event Completed
list.- (Backup and Compare schedules only) Event Compare Differences DetectedThe email addresses, separated by semicolons (;), to which notification will be sent if the compare finds differences between the specified backup data or configuration data version and the data on the physical device.
- Event CompletedThe email addresses, separated by semicolons (;), to which notification will be sent when the operation completes for the asset. If a Backup and Compare schedule completes without differences, an email is sent to this list. If it completes with differences, an email is sent to theEvent Compare Differences Detectedlist, not this list.
- Event FailedThe email addresses, separated by semicolons (;), to which notification will be sent if the operation fails.
(Backup and compare schedules only) Attach report to email
- Event Compare Differences DetectedThis defaults toTrueto attach a report of differences to the email if the backup and compare schedule finds differences between the specified backup data or configuration data version and the data on the physical device. SelectFalseto send an email without an attached report.
Provide Feedback