File Configuration dialog box
How do I open the File Configuration dialog box?
For a new schedule:
- Add a new schedule for a robot device.
- On the third page of the New Schedule Wizard, click in theFile Configurationfield and click
.
For an existing schedule:
- Click theSchedulesbutton to open theSchedulestab.
- Select the Backup or Backup and Compare schedule you want to edit.
- In the bottom left select the robot for which you want to change the file settings.
- In the bottom right, click in theFile Configurationfield and click
.
Use the
File Configuration
dialog box to specify which robot files to operate on in a Backup or a Backup and Compare operation. Because a robot contains many files, it can be more efficient to specify a default list of files or file types than to create the entire list for each operation. The default list (applied to new, not existing, schedules) is set from Tools > Options
. Changes made here override the defaults only for this schedule.Provide Feedback