Items in File Configuration dialog box

Items in the dialog box include:
  • Add
    Click to add a file or file type to the list. You can specify specific file names (like diocfgsv.io), file types (like *.vr for all files ending in .vr) or all files (*.*). Enter one file name or file type at a time. That is, click the
    Add
    button for each file name or type you wish to add.
    TIP:
    Motoman robot file configurations are based on each individual robot's hardware configuration and your operational needs. Before adding files to this list, we recommend that you consult with Motoman to obtain the specific list of files that meets your robot's configuration.
  • Remove
    Highlight the file name or type that you want to remove from the list and click
    Remove
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal