Change schedule timing
For Disaster Recovery schedules you can change when a scheduled operation runs. For Device Monitor schedules you can change the idle time and the maximum and minimum runtime (because Device Monitor schedules run continuously when active). You cannot change the type of operation a schedule performs. You would have to delete the schedule and create a new schedule.
Prerequisites
- To modify schedule run times, you must haveEdit a schedulepermission.
To modify a schedule's timing properties
- SelectView > Schedules, or click theSchedulesbutton.
- Before you can change the timing properties for a schedule, the schedule must be inactive. Clear theActivecheck box for the schedule you want to modify.
- In the schedule's row, click theTiming Propertiesfield and then click
.TIP:You can also select the schedule row and then click
. - Complete theNew Schedule Wizard: Timing Propertiesdialog box.
- ClickOK.
Provide Feedback