Comparison Overview dialog box
This dialog box shows an overview of the results showing which Siemens S5 or S7 Controller (STEP7) files had differences.
To show detailed results:
- Double-click an item in theObjectorDifference Typecolumn.
Compare partner 1
This is the item chosen as the first compare partner in the
Select Compare Partners
dialog box.This program is compared to the second program. Differences reported show whether something was changed, added, or deleted in this program relative to the second one. For example, if the report says an item was inserted, that means that the item was found in this program but not the second.
Compare partner 2
This is the item chosen as the second compare partner in the
Select Compare Partners
dialog box. Differences reported show whether something was changed, added, or deleted in the first program relative to this one. So if the report says an item was deleted, that means that the item was found in this program but not in the first one.Object
The
Object
column lists the contents of the folders or programs chosen as the compare partners.Difference Type
Describes the type of difference found in the object.
Difference Type | Meaning |
|---|---|
Different | A difference in the contents was detected. |
Not significant different | A difference was previously detected, but is no longer detected. |
Inserted | The object exists in Compare partner 1 but not Compare partner 2. |
Deleted | The object does not exist in Compare partner 1 but does exist in Compare partner 2. |
Provide Feedback