Block Options dialog box (Siemens)
How do I open the Block Options dialog box?
You can use the
Block Options
dialog box while setting default schedule properties or while editing the properties for a particular schedule.While setting default operation properties:
- SelectTools>Options.
- UnderCategoryon the left side of the dialog box, selectScheduled Operations.
- In theScheduled Operationstree, expandDisaster RecoveryandBackuporBackup and Compare.
- Select a Siemens S5 Controller, Siemens S7 Controller (STEP7), or Siemens S7 Controller (TIA Portal) device.
- Click in theBlock Optionsfield on the right and then click
.
For a particular schedule:
- Click theSchedulesbutton to open theSchedulestab.
- Select the Backup or Backup and Compare schedule you want to edit.
- In the bottom left, select the Siemens S5 Controller, Siemens S7 Controller (STEP7), or Siemens S7 Controller (TIA Portal) device for which you want to change the excluded blocks.
- In the bottom right, click in theBlock Optionsfield and then click
.
Use this dialog box to specify blocks that you do not want to include in the Siemens S5 or S7 Controller (STEP7) comparison.
Provide Feedback