Change logs refresh rate

The log shows new data at the refresh rate determined. You can change the number of seconds between refreshes.
To change logs refresh rate
  1. Select
    Tools > Options
    .
  2. Under
    Category
    on the left side of the dialog box, select
    Logs Viewer
    .
  3. In the
    Refresh Rate
    field, enter the time interval, from 5 to 60 seconds, at which all logs are refreshed.
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal