Comment dialog box
How do I open the Comment dialog box?
- SelectView > Logs(or click theLogsbutton).
- SelectView > Diagnostics & Health Log(or click theDiagnostics & Health Logbutton).
- Double-click the desired record row, or with the desired row selected, in the Log Item Details pane at the bottom of the log, click
. - ClickAdd New Comment.TIP:To show the Comment dialog box, you can also change the status of a Diagnostics & Health Log record.
Use the
Comment
dialog box to add a comment to a Diagnostics and Health Log record. Comments can be added as additional information regarding a Diagnostics & Health Log record, or when you change the status of a record. For example, you might want to add an explanatory comment regarding why a record was deferred or ignored.Provide Feedback