Specify addressing information for FactoryTalk Optix Runtime (Software)
You must be connected to the control network to specify addressing information for the device.
To specify the addressing information
- Open asset properties, click anywhere in theAddressing Infofield, and then click
. - Enter the IP address of the computer that FactoryTalk Optix Runtime software is running on.
- Enter the username and password for the FactoryTalk Optix Runtime software, and then selectOK.
- Complete the remaining fields as needed, and then selectOK.
Provide Feedback