Add FactoryTalk Optix Runtime (Software) dialog box
How do I open the Add FactoryTalk Optix Runtime (Software) dialog box?
- To enter theDesignmode if you are not already in it, click
. - In theAsset Catalog, expand theSCADA, EOI and FactoryTalk Itemsnode.
- Drag a FactoryTalk Optix Runtime (Software) asset onto the tree in the asset view.
Use the
Add FactoryTalk Optix Runtime (Software)
dialog box to add a FactoryTalk Optix
Runtime (Software) asset to the asset tree. You can add a FactoryTalk Optix Runtime (Software)
asset in the root or in a container.This asset allows you to run a schedule that backs up FactoryTalk Optix Runtime software on a
generic Windows or a Linux operating system. FactoryTalk Optix applications designed using
FactoryTalk Optix Studio 1.6.4 or later are supported. To ensure optimal performance and
compatibility with FactoryTalk AssetCentre, we recommend always applying the latest available
hotfixes for any version of FactoryTalk Optix Studio.
The device is added to the asset tree as soon as this dialog box opens. Clicking
Cancel
in this dialog box abandons any changes made to the device properties, but leaves the device in the tree.Provide Feedback