Event log messages when the connection to an Allen-Bradley Stratix Switch fails
When running a schedule on an Allen-Bradley Stratix Switch, the connection to the device may fail due to various reasons. To help you understand why the connection failed, the following table lists the messages recorded in the event log, their meanings, and the commands that FactoryTalk AssetCentre sends to an Allen-Bradley Stratix Switch.
Event log messages | Meaning |
|---|---|
Connecting to Allen-Bradley Stratix Switch using SSH IP Address, Port, User name and Password, RockwellAutomation.FTAssetCentre.Agents.DRStratixAgent.UI.StratixAddressingInfo: A connection attempt failed because the connected party did not properly respond after a period of time, or established connection failed because connected host has failed to respond. | The IP address of the SSH connection type cannot be connected to. |
Connecting to Allen-Bradley Stratix Switch using SSH IP Address, Port, User name and Password, RockwellAutomation.FTAssetCentre.Agents.DRStratixAgent.UI.StratixAddressingInfo: No connection could be made because the target machine actively refused it. | The IP address of the SSH connection type can be connected to but the designated device is not an Allen-Bradley Stratix Switch or the traffic on the specified port number is not permitted. |
Connecting to Allen-Bradley Stratix Switch using SSH IP Address, Port, User name and Password, RockwellAutomation.FTAssetCentre.Agents.DRStratixAgent.UI.StratixAddressingInfo: Socket read operation has timed out after 30000 milliseconds. | The specified port number is not for the SSH connection type but for the Telnet connection type or the port number is not for either of them. |
Connecting to Allen-Bradley Stratix Switch using SSH IP Address, Port, User name and Password, RockwellAutomation.FTAssetCentre.Agents.DRStratixAgent.UI.StratixAddressingInfo: Permission denied (password). | With the SSH connection type, the user account is deleted, the user name is not correct, or the user password is not correct. |
Unable to backup Allen-Bradley Stratix Switch because user 'admin' can only view status and monitoring information. |
|
Unable to backup Allen-Bradley Stratix Switch because the asset addressing info has not been set. | The addressing information is not configured. |
Connecting to Allen-Bradley Stratix Switch using Telnet IP Address and Port, RockwellAutomation.FTAssetCentre.Agents.DRStratixAgent.UI.StratixAddressingInfo: A connection attempt failed because the connected party did not properly respond after a period of time, or established connection failed because connected host has failed to respond IPAddress:PortNumber . | The IP address of the Telnet connection type cannot be connected to. |
Connecting to Allen-Bradley Stratix Switch using Telnet IP Address and Port, RockwellAutomation.FTAssetCentre.Agents.DRStratixAgent.UI.StratixAddressingInfo: No connection could be made because the target machine actively refused it IPAddress:PortNumber . | The IP address of the Telnet connection type can be connected to, but the designated device is not Allen-Bradley Stratix Switch. |
Connecting to Allen-Bradley Stratix Switch using Telnet IP Address and Port, RockwellAutomation.FTAssetCentre.Agents.DRStratixAgent.UI.StratixAddressingInfo: The returned string do not end with expected strings. | The specified port number is not for the Telnet connection type but for the SSH connection type or the port number is not for either of them. |
Connecting to Allen-Bradley Stratix Switch using Telnet User name and Password, RockwellAutomation.FTAssetCentre.Agents.DRStratixAgent.UI.StratixAddressingInfo: authentication failed . | With the Telnet connection type, the user account is deleted, the user name is not correct, or the user password is not correct. |
Connecting to Allen-Bradley Stratix Switch using Telnet User name and Password, RockwellAutomation.FTAssetCentre.Agents.DRStratixAgent.UI.StratixAddressingInfo: login invalid. | With the Telnet connection type, the user account is deleted, the user name is not correct, or the user password is not correct. |
Connecting to Allen-Bradley Stratix Switch using Telnet User name and Password, RockwellAutomation.FTAssetCentre.Agents.DRStratixAgent.UI.StratixAddressingInfo: The returned string do not end with expected strings. | The Allen-Bradley Stratix Switch is disconnected while the schedule is running. |
Provide Feedback