Stratix Switch Address dialog box
How do I open the Stratix Switch Address dialog box?
You can open the
Stratix Switch Address
dialog box while adding an Allen-Bradley Stratix Switch asset to the asset tree or while editing the asset's properties.While adding an asset to the asset tree:
- If you are not in Design mode, click
. - Drag an asset from the Asset Catalog to add it to the Asset View.
- Click anywhere within theAddressing Infofield, and then click
.
While editing an asset's properties:
- If you are not in Design mode, click
. - Double-click an asset in the asset tree.
- Click anywhere within theAddressing Infofield, and then click
.
Use the
Stratix Switch Address
dialog box to supply IP address, connection type, and user credentials for the physical device that you want to connect to and add as an asset.The following table lists the properties in the dialog box.
Properties | Descriptions |
|---|---|
IP Address | Enter the IP Address of the Stratix Switch. |
Port | Enter the port number connecting to the Stratix Switch. By default, the SSH connection type uses port 22 while the Telnet connect type uses port 23. Work with your system administrator to determine the correct port number. |
Connection type | Choose a connection type:
To determine which one to choose, you need to know the configured access to the Stratix Switch and if it's turned on. To check the enabled access, log on to the Stratix Switch Device Manager:
For detailed information about the Stratix Switch configuration, ask your system administrator. |
User name | Enter the user name to log on to the Stratix Switch. |
Password | Enter the password of the user name. |
Enable Password | Enter the password that is required to perform specific operations of a higher privilege within Stratix Switch. The Enable Password is a password that allows you to enter the privileged mode while managing the device where you can perform more operations that are not available on the level using just the Password. |
Test Connection | Click this button to validate whether the IP address, port number, connection type, and credentials are all correct.
Tip : In certain cases, after clicking Test Connection , the Stratix Switch Address dialog box stops responding before showing the connection failed message. You need to wait for several seconds for the system to be responsive. |
OK | Click to confirm all the information entered in this dialog box. It is only available when all the information is valid after clicking the Test Connection button. |
Cancel | Click to close this dialog box. No changes made will be saved. |
Help | Click to open Help. |
Provide Feedback