Add Generic FTP Device dialog box

How do I open the Add Generic FTP Device dialog box?
  1. If you are not already in Design mode, click design_mode_button.
  2. In the Asset Catalog, expand the
    FTP and Computer Device Items
    node.
  3. Drag a Generic FTP Device asset onto the tree in the Asset View.
Use the
Add Generic FTP Device
dialog box to add an FTP device to the asset tree. Use the Generic FTP Device asset to represent a robot or drive that uses FTP. You can add a Generic FTP Device in the root or in a container.
The device is added to the asset tree as soon as this dialog box opens. Clicking
Cancel
in this dialog box abandons any changes made to the device properties, but leaves the device in the tree.
TIP:
To perform Disaster Recovery operations on an FTP device containing subdirectories, the FTP device must support both the DIR and LS commands. To verify this, use Command Prompt in Windows to log on to the FTP device. Type
DIR
and press
Enter
. Then type
ls
and press
Enter
. Both commands should issue the same results.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal