Synchronize lifecycle status of assets
Synchronize the lifecycle information of assets in the FactoryTalk AssetCentre server with the Rockwell Automation lifecycle website. The lifecycle synchronization is recommended to run during server null time (time when no scheduled tasks or user interaction is taking place) if possible.
With the synchronization process being based on product ID or catalog number quantity, it can take some time to complete based on the total collected, and will require server resources during runtime.
The AssetCentre Server requires an Internet connection for this operation. If the network of your hardware devices has no Internet connection, configure a proxy on the FactoryTalk AssetCentre server computer. For more information, see
FactoryTalk AssetCentre Server Settings Utility Help
.To synchronize lifecycle status of assets
- SelectView > Assets Lifecycle, or click theAssets Lifecyclebutton.
- Click theAssettab.
- ClickSync. A progress bar shows.
- After the progress, the lifecycle information is updated to the FactoryTalk AssetCentre database and the lifecycle status is updated on the asset list.
Provide Feedback