Refresh lifecycle status of assets
Refresh the lifecycle information of assets on the FactoryTalk AssetCentre client with the FactoryTalk AssetCentre server. This operation doesn't need an Internet connection.
To refresh lifecycle status of assets
- SelectView > Assets Lifecycle, or click theAssets Lifecyclebutton.
- Click theAssettab.
- ClickRefresh. A progress bar shows.
- After the progress, the lifecycle information is updated from the FactoryTalk AssetCentre database to the client and the lifecycle status is updated on the asset list.
Provide Feedback