Export lifecycle information
You can export the lifecycle information to a CSV file. Depending on the tab (
Asset
or Asset Inventory
) you are on, you can export the lifecycle information of assets on the asset tree or included in the specified RAAI file.To export lifecycle information
- SelectView > Assets Lifecycle, or click theAssets Lifecyclebutton.
- Click theAssettab or theAsset Inventorytab.
- ClickExport.
- In theSave Asdialog box, specify the name of the CSV file and a path to save it.
- ClickSave.
Provide Feedback