Information in the export file
The following table lists the items in the CSV file exported from the
Asset
tab of Assets Lifecycle.Items | Description |
|---|---|
Path | The path of an asset or device as in the asset tree. |
Asset/Device Name | The name of an asset or device. The name of parent nodes such as container and the root node is also shown. |
Program Name | The name of project created in the controller. |
Manufacturer | The name of the company that offers a device. |
Product ID | The product ID of a device. |
Serial Number | The serial number of a device. |
Product Description | The product description of a device. |
Addressing Info | The device's location on the control network. |
Revision | The existing firmware revision in the device. |
Catalog Information | The catalog number of the device. |
Manufacture Date | The manufacture date of the device. |
Hardware Revision | The hardware revision of the device. |
Warranty Number | The warranty number of the device. |
Series | The series of the device. |
MAC Address | The MAC address of the device. |
Lifecycle Status | The lifecycle status of a device. |
Discontinued Date | The announced discontinued date. |
Recommended Replacement Product | The recommended product to replace the current one. |
Replacement Category | The nature of the replacement. |
Last Update Date | The last time when the life-cycle status was updated. |
Most Current Minor Release | The most current minor firmware revision available for the device. |
Most Current Release | The most current major firmware revision available for the device. |
The following table lists the items in the CSV file exported from the
Asset Inventory
tab of Assets Lifecycle.Items | Description |
|---|---|
Asset/Device Name | The name of an asset or device. The name of parent nodes such as container and the root node is also shown. |
User Comments | Comments that you can enter for each device or asset. |
Device Address | The network address of a device. |
Device Identity | The identity of a device. |
Path | The path of an asset or device as in the asset tree. |
Product Type Code | The product type code of a device. |
Revision | The existing firmware revision in the device. |
Serial Number | The unique serial number of the device. |
Program Name | The name of project created in the controller. |
Product Code | The identification code as defined in the device's EDS file. |
Product Name | The product name of a device. |
Product Type | The product type of a device. |
Vendor ID | The name of the company that offers the device. |
Network Type | The nature of the communication type of a device or asset. All communication items are identified as Bus, while all device items are identified as Device. |
Network Node Type | The network node type of the device. |
Catalog Information | The catalog number of the device. |
Manufacture Date | The manufacture date of the device. |
Hardware Revision | The hardware revision of the device. |
Warranty Number | The warranty number of the device. |
Series | The series of the device. |
MAC Address | The MAC Address of the asset. |
Commission Date | The commission date of the device. |
Product ID | The product ID of a device. |
Product Description | The product description of a device. |
Lifecycle Status | Life-cycle status of a device. |
Last Update Date | The last time when the life-cycle status was updated. |
Discontinued Date | The announced discontinued date. |
Replacement Category | The nature of the replacement. |
Recommended Replacement Product | The recommended product to replace the current one. |
Most Current Minor Release | The most current minor firmware revision available for the device. |
Most Current Release | The most current major firmware revision available for the device. |
Provide Feedback