Set Working Folders dialog box
How do I open the Set Working Folders dialog box?
- SelectView > Archive, or click theArchivebutton.
- In the asset tree, select an asset.
- On theArchivetab, after theWorking folderfield, clickSet.
Use the
Set Working Folders
dialog box to specify the working folder location. Setting a working folder for an asset sets the working folder for all files in the asset. The current working folder for the selected asset appears at the bottom of this dialog box.Provide Feedback