Items in Remove Label dialog box
Items in the dialog box include:
- Recursively remove labels from files and subfoldersSimultaneously remove labels from all files and files located in subfolders of the selected device, container, or folder. This option is available only if you select a device, container, or folder in the asset tree.
- LabelType the exact name of the label you want to remove from the file. If you cannot remember the label name, clickCanceland refer to the file'sHistorytab or theLabelstab to identify the label you want to remove.
- CommentsEnter an optional comment with the reason for removing the label. The maximum length for a comment is 2,500 characters.
Provide Feedback