About getting a file or binder

Get allows people who need to use the file (but don't need to edit it) to get the necessary version. For example, if you want to copy rungs from another ladder program, you can get that program (even if another user has the file checked out), copy the rungs, and then paste them into your file. Getting a file eliminates accidental changes to the master file.
FactoryTalk AssetCentre makes it easy to locate a file or binder that you get by duplicating the asset tree structure on your hard drive. The asset tree structure is duplicated from the container or folder where the working folder is set to the container or folder where the file or binder you are getting is located. The date and time a file is retrieved appears in the file history.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal