New Group dialog box
How do I open the New Group dialog box?
Do one of the following to open the
New Group
dialog box:
- SelectView>Address Book, click the dropdown arrow after theNewbutton, and then selectGroup.
- SelectTasks>Add New Address Book Group.
Use the
New Group
dialog box to create a group of contacts to receive simultaneous notifications regarding the progress and outcome of FactoryTalk AssetCentre schedules, tasks, and other system-related events.Groups cannot be imported from another email program. More than one user can create groups simultaneously.
Provide Feedback