Open the Asset Inventory window to view the scanning result

After running backup or backup and compare schedule on Asset Inventory, you can open the Asset Inventory window to view or edit the scanning result in grid view.
To open the Asset Inventory window
  1. Select
    View > Archive
    , or click the
    Archive
    button.
  2. In the asset tree, right-click the Asset Inventory backup file and select
    Open
    , or select the file in the asset tree and then at the top of the
    Archive
    tab, click the file link. The
    Asset Retrieval Options
    dialog box opens.
  3. In the
    Asset Retrieval Options
    dialog box, keep the
    Show in Asset Inventory Grid View
    check box selected.
    • If you want to open the Asset Inventory window in read-only mode, click the
      Get
      button. In read-only mode, you cannot edit the additional information or commission date for device assets. A read-only copy of the file is retrieved to the current working folder on your computer.
      TIP:
      To open the Asset Inventory window in read-only mode, you can also right-click a version of Asset Inventory asset's backup data on the
      History
      tab of
      Archive
      and select
      Asset Inventory View
      .
    • If you want to open the Asset Inventory window in editable mode, click the
      Check Out
      button. In editable mode, you can edit the additional information and commission date for device assets. A copy of the file is retrieved to the current working folder on your computer so that you can edit it.
      TIP:
      Clear the
      Show in Asset Inventory Grid View
      check box to get or check out a file as a normal backup file, without opening it in the Asset Inventory window.
  4. The
    Asset Inventory
    window opens.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal