Update assets in the asset tree with different asset properties
Once you have the Asset Inventory scanning result, you can update assets in the asset tree with different asset properties. You must enter design mode to update assets in the asset tree with different properties.
To update assets with different asset properties
- On theDevicestab in theAsset Inventorywindow, select theUpdateoption.
- Click theSYNCbutton.TIP:Clicking theSYNCbutton doesn't update any asset properties in the asset tree. It identifies assets in the scanning result that have different properties compared to assets on the asset tree.Make sure you are in design mode to proceed.After clicking theSYNCbutton, assets on theDevicestab that:
- exist in the asset tree with the same properties appear dimmed. The check boxes before them are automatically selected.
- don't exist in the asset tree appear dimmed. The check boxes before them are automatically cleared. You can add these assets to the asset tree using theAddoption.
- exist in the asset tree with different properties can be updated to the asset tree. The check boxes before them are available and are selected by default.
- Select the assets you want to update their properties to the asset tree. Click the
buttonon the toolbar. TheAsset Inventory Update Asset Wizarddialog box opens. - In theAsset Inventory Update Asset Wizard - Step 1 of 3dialog box, review the details of assets that will have their properties updated. ClickStart.
- In theAsset Inventory Update Asset Wizard - Step 2 of 3dialog box, a progress bar is shown while the updating operation is in process. If you want to cancel the operation, clickCancel.Usually, this step takes a very short amount of time unless you are updating a large amount of assets.
- When the updating process is complete, you can see result of the updating operation in theAsset Inventory Update Asset Wizard - Step 3 of 3dialog box. ClickFinish.To export the result, clickExportto save the result as a .csv or .txt file.Assets that have their properties updated to the asset tree appear dimmed on theDevicestab with check boxes selected before them.
Provide Feedback