Extraction using commands

The FactoryTalk AssetCentre Event Log Attachment Extraction supports execution using commands.
To extract event log attachment using commands
After configuring the settings for the extraction, a CONFIG file is created in the
AssetCentre Event Log Attachment Extractor
folder. The FactoryTalk AssetCentre Event Log Attachment Extractor uses this file for each extraction operation with a command. To change the settings, create a new CONFIG file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal