Use a command to start the extraction

Use FactoryTalk AssetCentre Event Log Attachment Extractor to extract event log attachments with a command without interacting with the software interface.
IMPORTANT:
Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").
Prerequisites
To extract event log attachments with a command
  1. Open the Windows
    Command Prompt
    window.
  2. Enter the full path of
    RA.FTAC.EventLogAttachmentExtractor.exe
    and the
    /S
    command. This command will start the extraction.
    For example,
    "C:\Program Files (x86)\Rockwell Software\AssetCentre Tools\AssetCentre Event Log Attachment Extractor"\RA.FTAC.EventLogAttachmentExtractor.exe /S
  3. Press
    Enter
    .
    The event log attachments and the operation report file are saved at the specified output location.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal