Create a CONFIG file
Before extracting event log attachments with a command, create a configuration file that includes all the settings for the operation.
TIP:
Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").
To create a CONFIG file
- Open the WindowsCommand Promptwindow.
- Enter the full path ofRA.FTAC.EventLogAttachmentExtractor.exeand the/Ccommand. This command opens the tool and allows you to further configure its settings.For example,"C:\Program Files (x86)\Rockwell Software\AssetCentre Tools\AssetCentre Event Log Attachment Extractor"\RA.FTAC.EventLogAttachmentExtractor.exe /C
- PressEnter.
- In theFTAC Event Log Attachment Extractordialog, configure all the settings.
- ClickOK.TheRA.FTAC.EventLogAttachmentExtractor.exe.configfile is saved at theAssetCentre Event Log Attachment Extractorfolder.
Provide Feedback