FactoryTalk AssetCentre Event Log Attachment Extractor

Use the
FactoryTalk® AssetCentre
Event Log Attachment Extractor to extract log file attachments when the
FactoryTalk AssetCentre
server experiences downtime or loses connection to the
SQL Server®
. This tool extracts log file attachments of the last run backup and compare task, which is supported on the user interface or through commands.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal