Database Limitations

  1. On
    Tools
    , select
    Database Management
    .
  2. On
    Database Management
    , select
    Database Limitations
    .
Use the
Database Limitations
to specify the settings of database limitations, including:
  • Total maximum size of the AssetCentre database
  • Size warning levels
  • Maximum number of versions per archive asset
  • Maximum size of database table capturing logs
  • Database capacity status refresh rate
  • Email notification
By default, the
Database Limitations Enabled
checkbox is not selected, and all the settings of database limitations are not available. To select the
Database Limitations Enabled
check box to configure all the settings, you must have the
Configure Database Limitations
permission.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal