Create a security posture check rule

Create a security posture check rule to monitor security-related configurations of Allen-Bradley Logix 5000 controllers.
Prerequisite
Make sure that you have the following permissions:
  • View Security Posture Check Rule
  • Configure Security Posture Check Rule
To configure permissions, go to
FactoryTalk Administration Console
>
Policies
>
Product Policies
>
FactoryTalk AssetCentre
>
Feature Security
>
Security Compliance Policies
.
To create a security posture check rule
  1. On
    Security Compliance
    , select
    Manage Security Posture Check rules
    .
    TIP:
    A default rule can be configured for all controllers. This rule cannot be deleted.
  2. Select
    Add rule
    .
    1. Enter a rule name.
    2. Select a desired controller from the dropdown list, and then enter a product string.
    3. Configure security posture check rules. You can toggle the specific group button to configure more rules. For more information, see Rule settings and Rule matching criteria.
  3. Select
    OK
    .
    TIP:
    By default, a rule will be activated after creation. Clear the checkbox next to the rule name to deactivate it.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal