Rule settings
The following table describes the settings of security posture check rules.
General | |
|---|---|
Controller mode | Select the controller mode of your device. The default value is set
to Run .
|
Key switch position | Select the position of the keyswitch of your device. The default
value is set to Run .
|
Major fault presence | Select the major fault status of your device. The default value is
set to Not present .
|
I/O forces presence | Select how the I/O forces capability is handled for your device. The
default value is set to Skip .
|
I/O forces state | Select the status of the I/O forces capability of your device. The
default value is set to Skip .
|
SFC forces presence | Select how the SFC forces capability is handled for your device. The
default value is set to Skip .
|
SFC forces state | Select the status of the SFC forces capability of your device. The
default value is set to Skip .
|
Firmware | |
Major version | Configure the major version of your firmware. Select >= or == to
define the version range, and then set the version number. For example, if the major version is 36:
|
Minor version | Configure the minor version of your firmware. Select >= or == to
define the version range, and then set the version number. For example, if the major version and minor version are 36 and 11:
|
Security | |
Change to detect bit mask | Select how the changes to detect capability is configured. By
default, this checkbox is not selected. If you select this checkbox, enter the bit mask. By default, all
items in the Changes to Detect list are selected for a
controller. The default bit mask is 16#FFFF_FFFF_FFFF_FFFF. |
Security authority state | Select the security authority status of your device. The default
value is set to Secured, but not bound to a security
authority .
|
Controller web pages | Select whether the access to the controller webpages is enabled. The
default value is set to Disabled .
|
Safety (Only applicable for safety devices) | |
Safety application state | Select the safety lock status of the safety application. The default
value is set to Skip .
|
Safety signature | Select the status of the safety signature. The default value is set
to Skip .
|
Protect signature in run mode | Select the status of the protect signature in run mode capability.
The default value is set to Skip .
|
Safety task major fault presence | Select the major fault status of the safety task. The default value
is set to Not present .
|
Provide Feedback