Source Controller Connection

FactoryTalk Analytics GuardianAI allows the user to configure a source controller to read the tags and monitor multiple component baselines based on the state value read from the PLC. This configuration is optional.
  1. On the
    Component overview
    panel, click
    Configuration
    . Each folder contains a Source Controller Connection page to connect to the Controller.
  2. The Source Controller Connection is divided into three sections, as follows:
    1. Controller Connection
    2. State Definition
    3. Monitoring On/Off
The user can select the tags for state definition based on the required. Tags with the icon are draggable and can be selected as tag for state definition and monitoring. Users can search for the required tags using the search bar and select the tags accordingly.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal