State Definition
On the
State Definition
page, the tags available in the added controller profile are
displayed. The tags are sorted in alphabetical order. Follow the below steps to define the
operational state of the component:- Select the required tags from the list view displayed. Only the lowest-level tags can be selected to define the different operational states of the component.The array tags can be expanded and the individual elements can be selected. The user can also search the required tags using the search functionality and select them as required.IMPORTANT: The boolean arrays are not supported in FactoryTalk Analytics GuardianAI.
- Drag and drop the selected tag to theSelected tagssection to define the operational states of the component.
- ClickSave. The "State definition configuration saved." message is displayed.
- ClickNext.State Definition

Provide Feedback