Monitoring On/Off

On the
Monitoring On/Off
page, the tags available in the added controller profile are displayed. The tags are sorted in alphabetical order. Follow the below steps to select a tag to determine whether the component should be monitored or not:
  1. Select the required tags from the list view displayed. Only the boolean tags should be selected.
    IMPORTANT: The boolean arrays are not supported in FactoryTalk Analytics GuardianAI.
  2. Drag and drop the selected tag to the
    Selected tags
    section to define the monitoring states of the component.
    NOTE: If there are no monitoring tags available in a nested tag,
    <No monitoring tags found>
    message is displayed under a parent tag.
  3. Click
    Finish
    . The "
    Source controller configuration saved.
    " message is displayed.
    Monitoring On/Off
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal