Add a new Drive and Component to Monitor

To add a new component to monitor, the user should complete the four steps summarized in the following diagram:
  1. Add and configure the variable frequency drive. Supported drives include Powerflex 755, 755TS/TL/TM/TR/HiHP and 6000T.
  2. Define the component to monitor (pump, fan, blower, motor for other component types).
  3. Configure training (define the minimum and maximum frequencies).
  4. Configure output controller to write the data back to the controller for operator notifications. This step is optional.
  5. Start the training process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal