Configuration Summary

After the configuration of Drive, Component, Training and Output Controller, FactoryTalk Analytics GuardianAI provides a summary page with final content validation. If any required field is missing, the configuration step is displayed with a yellow exclamation mark. Once all fields are completed and validated, click
Finish
to complete the new component configuration.
Once users finish the configuration, they are redirected to start training a baseline.
Configuration Summary and Validation
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal