Manage Firmware tab
The
Manage Firmware
tab lists revisions in all of the monitored folders.The following table explains each item on the
Manage Firmware
tab when ControlFLASH Plus
can access the Product Compatibility and Download Center.Item | Description |
|---|---|
Add Revisions | Opens the Add Firmware Revisions dialog box to search devices, and then select firmware revisions. To download firmware revisions, sign in to the Product Compatibility and Download Center. When no Internet connection is available, Add Firmware Revisions is not shown. |
Delete Revisions | Turns on the delete firmware revisions mode. Deleting unused firmware revisions improves the application's inventory building performance. |
Export Revisions | Opens the Save As dialog box to export the firmware inventory list. |
Device | Shows the individual catalog number of the device. When ControlFLASH Plus can access the Product Compatibility and Download Center and a device's firmware revisions are found in the Product Compatibility and Download Center, shows:
Tip : When a device's firmware revisions are all downloaded from the Product Compatibility and Download Center, disappears after refreshing the firmware.An orange highlight on the left border of this column indicates that a filter is active. |
Vendor | Shows the name of the device vendor. |
Lifecycle Status | Shows the device's lifecycle status found in the Product Compatibility and Download Center.
Tip : When there is no Internet connectivity to the Product Compatibility and Download Center, the lifecycle statuses are not shown.You can visit https://www.rockwellautomation.com/global/support/product-compatibility-migration/lifecycle-status/overview.page for more information. |
Revisions | Shows the following information:
|
File Path | Shows the file location of each firmware revision. Select a path link in the File Path column to locate the file in the monitored folder. When download starts, a progress bar appears. Select to cancel the download. Select to restart a canceled download. |
Filter by device | Filters one or more device types in a flashing session. The device list is filtered immediately as the text included in the device name is entered. The number of filtered devices and all devices shows on the left of the Filter by device box.An orange highlight indicates that a filter is active. |
Provide Feedback
shows:
to cancel the download. Select
to restart a canceled download.