Add Firmware Revisions dialog box
How do I open the Add Firmware Revisions dialog box?
- When searching the devices' firmware revisions by the catalog number, product family name, or bulletin number, selectAdd Revisions.
- When adding a specific device's firmware revisions, select
after the device's catalog number in the Devicecolumn.
When the Internet connectivity to the Compatibility and Download Center is available and you have signed in, use the
Add Firmware Revisions
dialog box to:- Search the devices as needed.
- Select and download the firmware revisions as found in the Product Compatibility and Download Center.
- View the firmware revisions' Release Notes and Important Notice as found in the Product Compatibility and Download Center.
Provide Feedback