Delete firmware revisions
Delete one or multiple unused firmware revisions in a single operation to improve inventory building performance.
Prerequisites
- Make sure the currently signed in user has permission to delete firmware revisions.
To delete firmware revisions
- On the Manage Firmware tab, select
to turn on the delete mode. - Select the checkboxes of firmware revisions that you want to delete.TIP:Select a device's checkbox to select all its firmware revisions. If you don't select all the firmware revisions of a device, the checkbox will appear dimmed.
- SelectDelete.TheDeletebutton appears dimmed when updating devices or downloading firmware revisions.
- When prompts, confirm the firmware revisions list.
- SelectDelete.If the deletion fails, check the permissions of the firmware.
Provide Feedback