ControlFLASH Plus overview

ControlFLASH Plus®
is a tool used for electronically changing firmware revisions in hardware devices. You can use this tool to:
  • Flash one or multiple devices within a single operation.
  • Manage firmware revisions and firmware locations.
  • Download firmware revisions from the Product Compatibility and Download Center.
  • Manage and use devices' revisions favorites.
  • Create an inventory of your devices and send the inventory to your
    Rockwell Automation®
    account for registration.
    IMPORTANT:
    ControlFLASH Plus
    only supports the firmware update for devices supporting the Common Industrial Protocol (CIP). To perform updates of non-CIP devices, use the
    ControlFLASH™
    tool.
Before using
ControlFLASH Plus
, you need to:
  • Install
    FactoryTalk® Linx
    version 6.60.00 and
    FactoryTalk® Services Platform
    version 6.60.00.
    TIP:
    There is an optional installation package that includes
    FactoryTalk Linx
    and
    FactoryTalk Services Platform
    in
    ControlFLASH Plus
    version 2.00.00 and later.
  • Configure communication drivers in the
    FactoryTalk Linx
    software.
  • Verify that your communications drivers work correctly.
We welcome your feedback about the Product Compatibility and Download Center. Contact us at https://compatibility.rockwellautomation.com/pages/FeedbackCC.aspx.
For more information about
ControlFLASH Plus
, visit Rockwell Automation Literature Library.
Rockwell Automation
recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal